{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the Power budget for AS, AS-P and IO modules?
PS-24V is the power supply for the SmartX AS-P servers, Automation Server, and I/O modules. The PS-24V power supply requires an input voltage of either 24 VAC +/–20 % or 24–30 VDC.

Use the power budget to calculate the maximum number of devices that the power supply, PS-24V, can supply. If more devices are used, additional power supplies must be added to the I/O bus. The power supply delivers and output voltage of 24 VDC +/– 1 V at an output current of about 1.25 A. The power supply can supply power for loads up to 30 W.
To determine the number and position of the power supplies, use the following power budget table.

Schneider Electric Nigeria