{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
what is SC3000 relay pack network wiring topology?
SC3000 relay packs can be connected to SER8300 line voltage room controller using one of the following topologies:
  1. Star Topology
  2. Daisy chain Topology
  3. Mixed Daisy Chained & Star Topology

NOTE:
  • A maximum of 10 SC3xxxE Relay Packs can be used for a single SER83xxA Room Controller.
  • Only the following models can be Slave Relays: SC3500E5045, SC3400E5045, and SC3300E5045.
  • Only one SC3x4X Relay Pack with monitoring input can be used for a single SERX3xxA Room Controller.

Schneider Electric Nigeria