{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the replacement for VW3A9212?
Issue:
VW3A9212 is not available, and what is the replacement?

Product Line:
ATV61, ATV71, ATV630, ATV930

Environment:
N/A

Cause:
Customer said the part is not available

Resolution:
If the
Conformity kit VW3A9212 is not available, then can use VW3A9112.  However, VW3A9112 is not UL Type 1 conformity kit but VW3A9112 is IP 21 conformity kit.

Schneider Electric Nigeria