Search FAQs
How can I reset fault using the STOP/RESET key of Graphic Display Terminal on the Altivar Process Drive?
Issue:
Is there a way to use the STOP/RESET key on the Graphic Display Terminal to reset Fault on the Altivar Process Drive?
Product Line:
Altivar Process Drive ATV630 ATV930
Environment:
All
Cause:
Customer would like to reset fault using the STOP/RESET key on the Graphic Display Terminal.
Resolution:
In order to press the STOP/RESET key on the Graphic Display Terminal to perform fault reset, active command channel is set to HMI.
Or:
Go to complete setting, then command reference, and scroll down to HMI cmd and set it to bumpless.
Toggle the LOCAL/REMOTE key to go to HMI, then press STOP/RESET to perform Fault Reset.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: