{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Power Monitoring Expert 9.0 / 2020: Report subscription UI shows wrong time (1-hour difference) than the configured time in case of PME system located in the region with ‘daylight saving’
Issue
While trying to modify the report subscription, it was observed that UI shows wrong time than the configured.



This issue exists in the PME 9.0 / 2020 systems located in the region with ‘daylight saving’ for example:


Environment
Power Monitoring Expert v9.0, v2020 system located in the region with ‘daylight saving’

Cause
Bug in the UI.


Resolution
Since the issue is only with the ‘Modify Subscription’ UI and same will be fixed in the upcoming CU releases, ignore this UI behavior of showing wrong time as the report subscription delivery continues to work with the configured value as same is stored in the RPT_Subscription table.


Note: Don’t change any configuration unless you want to configure different time.

Schneider Electric Nigeria