{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to Convert the a 32 bit Hex register in Modbus Tester to Decimal Value
Issue
Converting IEEE float to decimal

Product Line
Modbus Tester

Environment
Modbus register conversion

Cause
When using Modbus Tester to read a 32 bit register, the two 16 bit registers need to be converted in order to see the actual value.

Below is an example of reading 32 bit Input Registers:


Resolution
A converter such as https://babbage.cs.qc.cuny.edu/IEEE-754.old/32bit.html can be used.

The two hex values in each of the 16 bit registers are placed together to obtain the decimal value:


Modscan was used to validate the results:



Schneider Electric Nigeria

How to Convert the a 32 bit Hex register in Modbus Tester to Decimal Value
Issue
Converting IEEE float to decimal

Product Line
Modbus Tester

Environment
Modbus register conversion

Cause
When using Modbus Tester to read a 32 bit register, the two 16 bit registers need to be converted in order to see the actual value.

Below is an example of reading 32 bit Input Registers:
          

Resolution
A converter such as https://babbage.cs.qc.cuny.edu/IEEE-754.old/32bit.html can be used.

The two hex values in each of the 16 bit registers are placed together to obtain the decimal value:
          

Modscan was used to validate the results:
          


 

Schneider Electric Nigeria

Explore more
Range:
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Explore more
Range: