Search FAQs
Which meters in PM5000 series are compatible with Low voltage current transformers (LVCT)?
Issue
What meters in the PM5000 series are compatible with low voltage current transformers?
Product Line
PM5000 series meters
Environment
LVCT compatibility with PM5000 series meter
Cause
Compatibility question regarding PM500 series meter and LVCT
Resolution
LVCT (Low Voltage Current Transformer) can be used only with models PM5310R and PM5320R of the PM5000 series.
Note that PM5310R and PM5320R must be used with Schneider Electric’s “Quick Click” 3-in-1 LVCTs.
LVCTs cannot be used with any other models including PM5110, PM5560, PM5563, and more. For more information, refer to the PM5000 series technical data sheet here FA234024
What meters in the PM5000 series are compatible with low voltage current transformers?
Product Line
PM5000 series meters
Environment
LVCT compatibility with PM5000 series meter
Cause
Compatibility question regarding PM500 series meter and LVCT
Resolution
LVCT (Low Voltage Current Transformer) can be used only with models PM5310R and PM5320R of the PM5000 series.
Note that PM5310R and PM5320R must be used with Schneider Electric’s “Quick Click” 3-in-1 LVCTs.
LVCTs cannot be used with any other models including PM5110, PM5560, PM5563, and more. For more information, refer to the PM5000 series technical data sheet here FA234024
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: