{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Can I host RP-C controllers to Enterprise Server directly without AS-P?
Issue:
Is it possible to host RP-C controller to EcoStruxure Building Operation directly or it has to be hosted to AS-P?

Product Line:
EcoStruxure Building Operation, SmartX Room Purpose Controller (RP-C)

Resolution:
SmartX IP Controller - RP-C is a room purpose, fully programmable, IP based field controller. The RP-C models offer a flexible mix of I/O point types that suit a wide range of HVAC applications. The controller can either be used as a standalone BACnet/IP field controller or as part of an EcoStruxure BMS with a SmartX AS-P or AS-B server or an Enterprise Server as the parent server. 

1. RP-C Without RP expansion modules can be hosted directly to Enterprise server, AS-P, or AS-B, with the same limitations as other SmartX controllers, e.g. ES can host up to 600 RP-Cs Without RP expansion modules, but also consider that maximum number of hosted devices for all protocols is 600. Refer to architectural guidelines: https://ecostruxure-building-help.se.com/bms/Topics/show.castle?id=9266
2. For RP-Cs With RP expansion modules, they shall be hosted under AS-P only. Refer to the recommended architecture of RP-C with Expansion modules: https://ecostruxure-building-help.se.com/bms/Topics/show.castle?id=13067
 

Schneider Electric Nigeria

Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.