What are the criteria of tripping test of RCD according to IEC 61008?
RCCB (complying to IEC 61008) shall not trip at a current less than or equal to 0,5 IΔn, but it shall trip at IΔn within a specified time (see attached Table 1).
Released for:Schneider Electric Nigeria
Attachment(s)
Table 1 IEC 61008.jpg [106.86 KB]
Explore more
Range:
Vigi for Acti9 iC60
Acti9 iID
Vigi for Acti9 C120
Articles that might be helpful
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.