{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is EBO WebStation Kiosk mode and how to enable it?
Issue:
Want more information about WebStation Kiosk mode.

Product Line:
EcoStruxure Building Operation, WebStation

Resolution:
By enabling EcoStruxure Building operation WebStation Kiosk mode, toolbars will be removed. This mode is best used with SmartX HMI Kiosk, you can use SmartX HMI Kiosk to lock AD v3 in Kiosk mode to help prevent users from accessing an app other than the one you have selected.

WebStation without Kiosk mode:


WebStation with Kiosk mode:

To enable WebStation Kiosk mode, You can append the WebStation kiosk mode parameter to the IP address, ex. 192.168.42.116 /?kiosk# .

Schneider Electric Nigeria