{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How Current or Voltage Unbalance is calculated in Power Logic and ION meters?

Issue
The formula that calculates the percent Current or Voltage Unbalance in Power Logic and ION meters has not been mentioned in Manuals.

Product Line
Power Logic and ION meters that are in compliance with IEC 61000-4-30

Power Monitoring Expert 7.2.2
Power Monitoring Expert 8.2
Power Monitoring Expert 9.0
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
Power Monitoring Expert 2024

Environment
Power Monitoring Expert Vista Diagram, ION Setup, Technical Data sheet

Resolution
There are two commonly used definitions of Voltage Unbalance in the industry:

  1. NEMA Definition: NEMA stands for National Equipment Manufacturers Association in USA.

  2. True Definition: This definition of voltage unbalance is also known as ‘IEC Definition’ , â€˜True definition’ or â€˜Voltage Unbalance factor’.
     

According to IEC 61000-4-30 compliance and ION meters all PowerLogicâ„¢ and ION meters are compliant with the International Electrotechnical Commission's IEC 61000-4-30 (4-30) standard.

As per IEC 61000-4-30 the calculation of Unbalance is based on the following formula:
VU = (VN / VP)*100%
where:
V= Percent Voltage Unbalance
VN = Negative sequence voltage
VP = Positive sequence voltage

As per NEMA MG1-14.34, Voltage and Current Unbalance percentage is calculated based on the following formula:
I= 100 * max ( |I1 - Iavg| , |I2 - Iavg| , |I3 - Iavg| ) / Iavg
where:
Iavg = (I1 + I2 + I3) / 3 
max ( |I1 - Iavg| , |I2 - Iavg| , |I3 - Iavg| ) is the Maximum deviation from the mean value:
|I1 - Iavg| = abs(I1 - Iavg)
|I2 - Iavg| = abs(I2 - Iavg)
|I3 - Iavg| = abs(I3 - Iavg)

Voltage Unbalance is calculated the same as Current Unbalance formula based on NEMA method.

Example:
Iavg = (165.8 + 152.7 + 166.6) / 3 = 161.70
Maximum deviation from the mean value =  max( abs(165.8 - 161.7) , abs(152.7 - 161.7) , abs(166.6 - 161.7) ) = max( abs(4.1) , abs(-9) , abs(4.9) ) = max( 4.1 , 9 , 4.9) = 9
I= (9 / 161.70) * 100 = 5.5658 ~ 5.6
diagram example 
 

Schneider Electric Nigeria

Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.