{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Why the BMENOP0300 module show invalid configuration and the Modicon IEC61850 configuration tool validation is Pass with no errors?
Issue:
Why the BMENOP0300 module show invalid configuration and the Modicon IEC61850 configuration tool validation is Pass with no errors?

Product Line:
Modicon M580 Controller, BMENOP0300, NOP

Environment:
All

Resolution:
The BMENOP0300 module requires the Data Dictionary (Mandatory) and used the PLC embedded data.

Make sure that “Only HMI Variable” is not checked under project settings. If this option is checked that means only the selected variables allow to use of the PLC embedded data and the DDT related to the NOP might be not selected and this is one of the reasons that cause the device DDT of BMENOP0300 modules shows the invalid configuration. BMENOP0300 module fails at the parsing period (When NOP received the CPU’s config files) and it won’t start further tasks and will cause the issue.

The upcoming version of the Control Expert will highlight the warning or error message when “Only HMI Variables” is selected along with the BMENOP0300 Module

Schneider Electric Nigeria