{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to verify the BMXNOR0200H NTP Client service status inside the Control Expert application?
Issue:
How to verify the BMXNOR0200H NTP Client service status inside the Control Expert application?

Product Line:
Modicon M580 Controller, M340, BMXNOR0200H, BMXNOR0200.

Environment:
All

Resolution:
We can use the implicit exchange using the IODDT of type T_COM_ETH_BMX as described below and verify the NTPC_STATUS_BIT #5.
Note: This status bit tells only whether the BMXNOR0200H NTP Client service is activated configured and running or not. It will not tell the NTP Server connection status.

Schneider Electric Nigeria