{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Power Monitoring Expert - Reset supervisor password without sysadmin level SQL credentials
Issue
How to change the supervisor password with a user that does not have sysadmin role in SQL.

Product Line
Power Monitoring Expert 9.0
Power Monitoring Expert 2020

Environment
Reset Account - Installer

Cause
The account provided to connect to the database during the changing process has to have enough privilege to access and modify the ION_Network database under the security context.

Resolution
This can only be achieved by providing a SQL credential that has sysadmin as a role or that is "dbowner" of PME databases, which will be the "ION" login - assuming PME was installed in a Mix-Mode Authentication.



Additional Note
During install time you have the option to choose this password in the "Database Accounts" step. If this wasn't given, PME will autogenerate a password and you must have a sysadmin to be able to reset them.

Schneider Electric Nigeria