{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Video: How to Configure Emergency Egress Function in Security Expert.

Issue:
Need to configure Emergency Egress function in Security Expert.

Product Line:
EcoStruxure Security Expert

Resolution:
Emergency Egress is a built in Programmable Function in EcoStruxure Security Expert.  It is typically triggered by the fire alarm system within a building which is connected to the Security Expert system through any programmed input. Once activated, the function will immediately unlock all doors that are defined in the Emergency Egress door group and prevent anything from locking them again. When the fire alarm is reset, the Emergency Egress function secures all doors in the group.
Note: The Emergency Egress function is not intended to replace the emergency door release devices located at individual doors on the egress path, but instead to aid in an expeditious evacuation

The below video shows how to configure Emergency Egress in Securit Expert:


Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: