How can we help you today?

PME2020/ Energy Expert 3.0 How to enable the Multi-Use Token Functionality

Section 1 – Product /System/Environment information
EcoStruxure™ Energy Expert 3.0 Solution Guide
Energy Expert 3.0
Power Monitoring Expert 2020

_____________________________________________________________________________________
Section 2 – Issue
There is a mistake in the documentation EcoStruxure™ Energy Expert 3.0 Solution Guide on page 183. ( It has been observed that row is duplicated  instead of updated)

The SQL script does not enable the multi-use token
EXEC
ApplicationModules.Configuration.WriteConfigurationValue 'Web Framework','Server','MultiUseTokenEnabled',NULL,'true', 'GlobalSetting'
_____________________________________________________________________________________
Section 3 – Steps to Reproduce the Issue /Investigation/
How to check if Multi-Use Token is enabled

  • The functionality is by default disabled
  • Must be set “True” in the ApplicationModules database, Configuration table (System stored procedures


SELECT TOP (1000) [ItemType]
,[Item]
,[Key]
,[Value]
,[UserId]
,[Description]
FROM [ApplicationModules].[Configuration].[ConfigurationSettings]
where ItemType = 'Web Framework'
and Item = 'Server'
and [Key] = 'MultiUseTokenEnabled'


_____________________________________________________________________________________
Section 4 – Root Cause

  • Incorrect documentation

_____________________________________________________________________________________
Section 5 – Solution
How to enable the Multi-Use Token Functionality

UPDATE
[ApplicationModules].[Configuration].[ConfigurationSettings]
set Value = 'true' , [UserId] = 'GlobalSetting'
where ItemType = 'Web Framework' and Item = 'Server' and [Key] = 'MultiUseTokenEnabled'


After the authentication is enabled, use a web browser to navigate to:
https://<YourServerName>/Web/MUT.

Image_001

Schneider Electric Nigeria

Explore more
Category:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: