{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is cable type for connection between motor and softstarter PTC terminal block ?
Some practical recommendations for the type of cables that should be used are as follows:

- Distances ≤ 20 m – Standard parallel cable is acceptable
- Distances ≥ 20 m, ≤100 m – Twisted pair cable is necessary
- Distances ≥ 100 m – Screened twisted pair (STP) cable is necessary
- High level of interference  – Screened twisted pair (STP) cable is necessary

Schneider Electric Nigeria