{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can I upgrade Automation Server classic (AS) to EBO V3.2 or higher?
Issue:
Need to upgrade EBO project to V3.2 or higher but I have Classic Automation Server (AS)

Environment:
EcoStruxure Building Operation

Resolution:
EBO V3.2 or higher releases are not supported on the original AS’s often referred to as AS classic. From version 3.1 of EcoStruxure BMS it is possible to use a multi-version system, so you can keep AS to EBO V3.1.2 and upgrade other a servers (EC, ES, AS-P and AS-B) to EBO V3.2 or higher. Check below architecture as example:

Schneider Electric Nigeria