Search FAQs
Modbus register list for SLP series Temperature sensors and Humidity sensors
Issue:
Need Modbus register list from SLP series Temperature sensors and Humidity sensors
Environment:
SpaceLogic Room Units
Resolution:
The SpaceLogic SLP Series of air quality sensors for living space is a flexible multisensor platform for use with BAS controllers designed to accept BACnet or Modbus outputs.
Function Code:
Note that an attempt to write to “read only” holding registers will give an error and the entire write command will not be executed even if writing to read/write locations were also requested. Exception code 2 is given in this case. “Preserved” means the values is maintained through power outages.
![Input Register](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000009FnzTQAS&oid=00DA0000000abSm)
![Holding Registers](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000009FnzZQAS&oid=00DA0000000abSm)
Need Modbus register list from SLP series Temperature sensors and Humidity sensors
Environment:
SpaceLogic Room Units
Resolution:
The SpaceLogic SLP Series of air quality sensors for living space is a flexible multisensor platform for use with BAS controllers designed to accept BACnet or Modbus outputs.
Function Code:
Note that an attempt to write to “read only” holding registers will give an error and the entire write command will not be executed even if writing to read/write locations were also requested. Exception code 2 is given in this case. “Preserved” means the values is maintained through power outages.
Released for:Schneider Electric Nigeria
Explore more
Category:
Range:
Explore more
Category:
Range: