{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Configuration Manager Tool 2020 - "No matching constructor found on type" error when launching the tool

Issue
When first launching CM Tool 2020 on a server (usually older versions of OS) it will ask for .NET 4.6 to be installed as it is not present. After installing the .NET and rebooting the server the CM Tool will still fail to open and will throw the following error:
"No matching constructor found on type
'ConfigurationManager.ViewModels.ConfigurationManagerVM'. You can use the Arguments or FactoryMethod directives to construct this type.
"



Product Line
Configuration Manager Tool 2020

Environment
Upgrades
Migrations

Cause
This issue happens due to a missing .NET framework component.

Resolution
1) Apply all the outstanding Windows Updates on the server
2) Install .NET 4.7.2 framework

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: