I am missing the "Display on Map" menu option from object menu when right clicking on database objects. I have a working map set with map sources already configured.
Solution:
The Default Map Source is not configured on the Root object. Please right click on the Root object and select Edit Properties. The Default Map Source could be configured under the Geographic Information tab,
Released for:Schneider Electric Nigeria
Explore more
Product:
GEOSCADAEXPERT
Articles that might be helpful
Show more articles
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.