{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
In PME VISTA Voltage L-N data logging is not available for ION meters.
Issue
In PME, In VISTA Voltage L-N data logging is not available for ION meters.


Product Line
PME8.2, PME 9 & PME 2020 & ION meters (PM8000, ION7650, etc).

Cause
In PME VISTA application Voltage L-N data logging is not available for ION meters. This is because if the meter is installed in the star network then L-N reference will not be available so the by default only Voltage L-L is enabled.


Resolution
Please follow the below steps to enable log Voltage L-N logs, there are two areas where the changes must be made.
  1. In ION meter data recorders must be configured.
  2. Then in PME VISTA data logger to be modified.
  3. Please follow the steps in the attached document.

Schneider Electric Nigeria

Attachment(s)
IONmeters_VoltageLN_DataRecorderProcedure_InPME.pdf [1.86 MB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.