{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the single phase Altivar drives be used on single phase motors?

Article available in these languages: Spanish

Issue:
Could not find a drive to work with a single phase motor.

Product Line:
Altivar Machines

Environment:
All models and serial numbers

Cause:
N/A

Resolution:
All AC drives sold by SquareD Schneider Electric in the US are for use with 3 phase motors only. The single phase units are for use with single phase input only.

Schneider Electric Nigeria