Search FAQs
Does the Altistart ATS46 ATS48 ATS22 have any leakage voltage across the output terminals when unit is not running and what is the value?
Issue:
Does the Altistart ATS46 ATS48 ATS22 have any leakage voltage to the output?
Product Line:
Altistart ATS48 ATS22
Environment:
All models
Cause:
Measuring voltage on T1T2T3
Resolution:
The ATS46, ATS48 and ATS22 units do have leakage voltage across the output of the SCRs when it is not running. If the motor is connected, this minimal power is dissipated in the motor windings and not noticed. If the motor is not electrically connected to T1T2T3, this leakage voltage has the capability to reach the line potential.
Does the Altistart ATS46 ATS48 ATS22 have any leakage voltage to the output?
Product Line:
Altistart ATS48 ATS22
Environment:
All models
Cause:
Measuring voltage on T1T2T3
Resolution:
The ATS46, ATS48 and ATS22 units do have leakage voltage across the output of the SCRs when it is not running. If the motor is connected, this minimal power is dissipated in the motor windings and not noticed. If the motor is not electrically connected to T1T2T3, this leakage voltage has the capability to reach the line potential.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: