Search FAQs
What is the replacement coil for the electrically held 8903L lighting contactor?
Issue:
Replacement coils for 8903 Type L contactor:
Product Line:
8903 type L Lighting contactors
Environment:
North American Product
Cause:
Maintenance
Resolution:
This depends on pole quantity and voltage:
2-6 poles, 9998L**
7-12 poles, 9998LH**
* - use a 60 Hz coil of the next higher voltage
Replacement coils for 8903 Type L contactor:
Product Line:
8903 type L Lighting contactors
Environment:
North American Product
Cause:
Maintenance
Resolution:
This depends on pole quantity and voltage:
2-6 poles, 9998L**
7-12 poles, 9998LH**
Poles | Coil Class and Type | HZ | Suffix Number (complete coil number consists of the class and type followed by the suffix) | Coil VA | ||||||||||||
24v | 110-115v | 120v | 208v | 220v | 240v | 277v | 380v | 440v | 480v | 550v | 600v | Inrush | Sealed | |||
2-6 | 9998L | 60 | 23 | - | 44 | 50 | [*] | 53 | 55 | - | - | 62 | - | 65 | 150 | 30 |
50 | 24 | 44 | 45 | 52 | 53 | 54 | - | 60 | 62 | 63 | 65 | 66 | 140 | 30 | ||
8-12 | 9998LH | 60 | 23 | - | 44 | 50 | [*] | 53 | 55 | - | - | 62 | - | 65 | 180 | 35 |
50 | 24 | 44 | 45 | - | 53 | 54 | - | 60 | 62 | - | 65 | - | 170 | 35 |
* - use a 60 Hz coil of the next higher voltage
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: