{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the measurement accuracy of the Micrologic 5.0P, 6.0P, 7.0P, 5.0H, 6.0H, and 7.0H trip units (including the sensors)?

Product Line
Circuit Breakers

Resolution
Voltage (V): 0.5%
Current (A): 1.5%, higher accuracy (1%) can be achieved with special calibration on the current transformer (CT characterization option)
Frequency (Hz): 0.1 Hz
Power (W) and Energy (Wh): 2.0%, 1.5% if CT characterization is used

Note: The accuracy of the current measurements depends on both the value displayed (or transmitted) and the circuit breaker rating, where: Accuracy = 0.5% In + 1.5% reading
  • Example:For a circuit breaker with a 4000 A rating and a current displayed on Micrologic of 49 A, the accuracy is: 0.5 % x 4000 + 1.5 % x 49 = ±21 A

Schneider Electric Nigeria