{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
When using preset speeds and an analog speed input which one takes priority?
When the inputs for the preset speeds are high they override the analog speed. If the preset speed inputs are low then the drive will run at the analog speed input speed or LSP if no signal is present.


CTA-ID : 2001374

Schneider Electric Nigeria

Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.