{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Do the 9070 industrial control transformers conform to the IEC standard EN61558-1?

Issue:
IEC standard for 9070 transformers

Product Line:
Class 9070

Environment:
Control power transformers

Cause:
Codes

Resolution:
Yes, 9070 Control power transformers do conform to EN61558-1.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: