{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What could be the reason of getting all LED flashing at startup of BMENUA0100 ?
During the startup sequence, all the BMENUA0100 LED can flash all together and the module is not starting. It’s not possible to access to it.
BMENUA0100 Firmware version 1.10.25
One of the root causes of this behavior is that the rotary switch position is not well set, and it could be on an intermediate position.

Here is the position that can be set:
rotary switch
Example of rotary switch position that is not correct:
not good position

Schneider Electric Nigeria

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: