Search FAQs
How many numbers of channels supported by BMENOR2200H in the IEC104 Server Configuration?
The BMENOR2200H supports a maximum of 4 channels when configured as IEC104 server configuration.
![](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000009O81gQAC&oid=00DA0000000abSmMAI)
![](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000009O86WQAS&oid=00DA0000000abSmMAI)
Note:
Note:
- There is one main channel and the rest 3 of them are the virtual image of the main channel.
- The events in all 4 channels are not synchronized among them. Duplicated across all 4 channels
- To avoid the duplicated events the BMENOR2200H supports the IEC104 Server channel redundancy feature.
Released for:Schneider Electric Nigeria
Explore more
Product:
Explore more
Product: