{}

Our Brands

Impact-Company-Logo-English Black-01-177x54
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.
How can we help you today?
How to change the operating mode (Standard to Secured and vice versa) of the BMENOR2200H module?
In order to change the BMENOR2200H module from Standard mode to Secured mode. Or from the Secured mode to the Standard module the following steps must be followed.

NOTE:
  • It is not possible to change the mode directly from Secured to Standard and Standard to Secured. The module must be Factory Reset first in order to change the operating mode.
STEPS: (Let's assume the module is running in the Standard mode and we would like to change into the Secured mode)
  1. Removed the module from the backplane.
  2. Using the rotatory switch from the behind of the module and changed its position to the RESET. (Module will enter into the Factory reset state).
  3. Put back the module into the backplane and wait for the LEDs to lit ON. (The LED's indicated that the existing configuration is cleared and the module is now in Factory Reset state)
  4. Removed the module from the backplane.
  5. Using the rotatory switch from the behind of the module and change its position to the SECURED.
  6. Put back the module into the backplane.
  7. Now the module operates in a Secured Mode.
  8. Same steps are needed when changing from Secured mode to the Standard mode.
NOTE: By default, the module is in the secured mode from the factory.










Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.