{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can you download a different version of SoMove Configuration file in Altivar Process VFD?
Issue:
Can SoMove Software download an older Configuration file in to the VFD?

Product Line:
ATV630 , ATV930

Environment:
Altivar

Resolution:
You can download a SoMove Conf with version N to a drive with version N or N+1 or greater. but you can't transfer it to a drive with version N-1 or less.

You have 2 solutions inthe example below:

1.    You can modify the version of the offline conf, by changing the Topology.
Drive screen shot

Then click ok when SoMove displays message.

warning screenshot
After that, transfer the conf with version V2.2 to a drive with version V2.2.

Or

2.    Update the drive to the version V3.1 before transfer. Then you can perform conf transfer.

Schneider Electric Nigeria