{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the maximum surge current (VA rating) of the relay output modules BMXDRA0805 and BMXDRA0815?
The maximum surge VA rating for the BMXDRA0805 is 1250 VA.
The maximum surge VA rating for the BMXDRA0815 is 2000 VA.

This information was not available in the Modicon x80 Discrete Input/Output Modules User Manuals,
part number 35012474, dated 10/2019 or earlier.


Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: