{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Configuration Manager Tool - Error during Write to System "An error occurred while parsing EntityName"

Product Line
Power Monitoring Expert 2020
Power Monitoring Expert 9.0
_____________________________________________________________
Environment
Configuration Manager Tool 2020
Configuration Manager Tool 9.0
_____________________________________________________________
Issue

The Write to System task was completed but in the CM tool log there is an error like this:

|Exception occurred while writing System Registry.||Business
17:16:42:839||Information||None||System Registry||Exception Message An error occurred while parsing EntityName. Line 5329, position 33..||Business

_____________________________________________________________
Root Cause

The error was during Write to System due to an invalid character - ampersand "&" in the Registry.xml
Part of the registry with the offending entry:
<Value name="Installation Date & Time" value="30/04/2019 14:56:42" type="String" />
_____________________________________________________________
Proposed Solution

Extract the archive and remove the line from the registry.xml and then zip again.
The line number to be removed is going to be in the CM Tool log error message.
For instance:
17:16:42:839||Information||None||System Registry||Exception Message An error occurred while parsing EntityName. Line 5329, position 33..||Business


image.png

_____________________________________________________________
Additional Note

This issue may have impacted earlier versions of the tool. The resolution will be the same.
This issue has been fixed in Configuration Manager Tool 2021 onwards.

Schneider Electric Nigeria

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: