{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the BMXDDI3203 and BMXDDI3232 discrete input modules be used with Control Expert 15?
The BMXDDI3203 and BMXDDI3232 can be used with Control Expert 15.  The two input modules were released after CE15 was released and therefore requires a HotFix to be installed to allow their selection in the New Device IO Module pick list.

The HotFix file is 'ControlExpert_V150_HF_DDI_3232_DDI_3203.zip.' (see attachment)

The two extracted filenames are:
ControlExpert_V150_HF_DDI_3232_DDI_3203.exe
ControlExpert_V15_HF_DDI_3232_DDI_3203_ReadMe.mht


Follow the directions in the ReadMe to install the HotFix in Control Expert 15.

Schneider Electric Nigeria

Attachment(s)
ControlExpert_V150_HF_DDI_3232_DDI_3203.zip [11.54 MB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: