{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
PME 2020 - PQ Tolerance Chart wrong x-axis sequence

Product Line

Power Monitoring Expert 2020

_____________________________________________________________________________________

Environment

Web Application - Alarms - Tolerance Chart ITIC/CBEMA

_____________________________________________________________________________________

Issue

The tolerance chart for a PQ event in Alarms is plotted wrong.

The x-axis has a wrong sequence and the event is plotted in the wrong place according to the graph x-axis.

The x-axis sequence in the graph is displayed as 1 MC - 100 MC - 10 MC - 1000 MC

The value plotted is 429 MC in the image.

_____________________________________________________________________________________

Steps to Reproduce the Issue /Investigation

1 - Change the Web App language to Russian

2 - Select a PQ event from the Alarm and double click

3 - Click on Tolerance Chart

The x-axis sequence in the graph in the English language is: 1 μs - 100 μs - 10 ms - 1000 ms

_____________________________________________________________________________________

Root Cause

PME translated microseconds in the same way as milliseconds "мс".

____________________________________________________________________________________

Troubleshooting/Proposed Solution

1) Backup PME databases

2) Run the following query in SSMS

Update [ApplicationModules].[Internationalization].[LocalizedStrings]

Set LocalizedValue = '{0} μs'

where LanguageSpecifier = 'ru' and ResourceKeyname = 'Time_Units_microsecond_1'

3) Refresh Web Application

____________________________________________________________________________________

Additional Notes

This issue has been fixed in PME 2021.

Schneider Electric Nigeria

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: