Search FAQs
Masterpact MTZ: How to create a CT test position cradle contact.
Issue: The eIFE uses same physical position as the CT test position chassis contacts.
Product Line: Circuit Breakers
Environment: Masterpact MTZ chassis
Resolution:
Wiring a CD xx1-xx2 in series with a CE xx1-xx4 creates a simulated CT contact. Same as a CT xx1-xx2 contact.
![image.png](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000009ld6oQAA&oid=00DA0000000abSmMAI)
Product Line: Circuit Breakers
Environment: Masterpact MTZ chassis
Resolution:
Wiring a CD xx1-xx2 in series with a CE xx1-xx4 creates a simulated CT contact. Same as a CT xx1-xx2 contact.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: