Search FAQs
Using both CREATE_FILE and OPEN_FILE returns error 21.
If you configure the CREATE_FILE, OPEN_FILE, WR_DATA_TO_FILE and CLOSE_FILE to create or open a file on the M340 or M580 data storage SD card, attempts to perform either a write to the file or close the file without properly considering the usage of the FILEDESC output on both the CREATE_FILE and OPEN_FILE blocks , will results in an error 21 getting returned..
![image.png](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000009sGrdQAE&oid=00DA0000000abSmMAI)
This is due to the output of the OPEN_FILE block over writing the output of the CREATE_FILE block.
To resolve the issue, the following logic can be used as an example on how to configure the OPEN_FILE and CREATE FILE.
This is due to the output of the OPEN_FILE block over writing the output of the CREATE_FILE block.
To resolve the issue, the following logic can be used as an example on how to configure the OPEN_FILE and CREATE FILE.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: