{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
PME 2020 - Hourly Usage Report has the timestamps shift by 1 hour

Product Line

Power Monitoring Expert 2020
Power Monitoring Expert 2021

_____________________________________________________________

Environment

Web Application - Report - Hourly Usage Report

_____________________________________________________________

Issue

Timestamps are shifted by +1 hour in the Hourly Usage Report.

In PME 9.0, in the below image, the timestamp is correct:

In PME 2020, in the below image, the timestamp is shifted by 1 hour:

_____________________________________________________________

Root Cause

The report is treating the data as interval end instead of interval beginning.

_____________________________________________________________

Proposed Solution

1) Make a copy of the Hourly Usage Report.rdlc located at %\Power Monitoring Expert\web\ReportDepot\ION Reports\ION Report Packs\Default Reports

2) Open the original rdlc file with a XML editor (Notepad, Notepad++, etc).

3) Crtl+F to find "DateAdd" string

4) Edit lines 1457 and 1459, changing respectively 59 and 60 to -1 both.

5) Save the file and run the report again

_____________________________________________________________

Additional Notes

This issue has affected PME 2020 and PME 2021.
Although the resolution above is applicable for both versions, an official hotfix will be provided for PME 2021 and added to this article when available.

Schneider Electric Nigeria

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: