{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Adding an Ethernet module (BMXNOC040x, 140NOC78xxx ) causes Control Expert 15 to close.
Adding a BMXNOC040x or 140NOC78xxx to the applicable rack will return the following error message.  This will be followed by an unexpected closure of Control Expert 15.






This issue will occur if the module is added to a Control Expert application after installing the following hot fixes
  • 'ControlExpert_V150_HF0380584E'
  • ControlExpert_V150_HF_Integrity_Check'


This issue applies to the following DTM related modules::

M580 :
  • BMXNOC0402


M340 :
  • BMXNOC0401
  • BMXNOC0401.2


Quantum :
  • 140NOC78100,
  • 140NOC78100.2,
  • 140NOC78000,
  • 140NOC78000.2


The following steps can be used as a workaround,
  • Uninstall Control Expert.
  • Reinstall Control Expert.
  • Install all hot fixes except 'ControlExpert_V150_HF0380584E'.


This issue will be fixed in a soon to be released hot fix.

Schneider Electric Nigeria