{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is Resi9 MP made of recycled plastic?
Issue:
I'm searching for a Resi9 MP enclosure using recycled plastic.

Product Line:
Resi9 MP

Resolution:
Yes, Resi9 MP flush back part for standard installation (not hollow wall) is made of recycled plastic.

Notes:
To select the right enclosure, please select the product with the commercial reference starting with MIP20 or MIP22.

Schneider Electric Nigeria