{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the range of Wiser devices?
Technical specification of ZigBee states that the range is between 10-100m (line-of-sight). However, this is the "laboratory environment" value and is greatly affected by a number of factors; interference, environment, obstacles etc..
It is generally accepted that the indoor transmission distance is 10-20m.
The strength of ZigBee and Wiser is in the meshing functionality - every wired (mains powered) ZigBee device acts as a range extender.
The whole ZigBee network is then automatically built in a way that guarantees strongest possible signal bonds between the devices.
This means that every wired device extends the overall signal coverage of the whole system!

Here's a snippet from the System User Guide (p. 17) that explains this concept nicely:

On one hand, negative properties of the environment might make it a lot less that those "ideal" 100m; on the other hand, the meshing mechanism makes the range much, much more.

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: