{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
NetBotz 4.x firmware: TLS auto-negotiates to the highest version
Issue:
TLS auto-negotiates to the highest version

Product Line:
NetBotz

Environment:
Botsware version 4.5.2 to 4.7

Cause:
TLS versions 1.0, 1.1, and 1.2 are available on a number of versions of NetBotz firmware. Version TLS 1.2 was added in version 4.5.2 and TLS 1.0 was removed in version 4.6.4

Resolution:
Although version 1.1 is still available, whatever system connects to the NetBotz appliance should auto-negotiate to the highest version of TLS available on both systems. If your browser is capable of 1.2 and your NetBotz appliance is running firmware 4.5.2 or higher, the connection should be made using TLS 1.2.

Schneider Electric Nigeria