{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does the EcoStruxure OPC UA server Expert support extracted bits of a integer ?


Issue:
Support of extracted bits for Variables with Data Type INT or UINT


Product Line:
OPCUAServerExpert V2.01 SP1, M580


Resolution:
Yes. With Ecostruxure OPC UA Server Expert V2.01 SP1 it is possible to address an extracted bit of a Variable with Data Type INT or UINT. For instance, to address the extracted bit 4 of a Variable with NodeID "s=0:M580!MyVar", address the NodeID "s=0:M580!MyVar.4"

Schneider Electric Nigeria