{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
My LoRa network is weak so I need to use the 5 meters cable extender in order to place the antenna of PrismaSeT Active in a better network-covered place. What is the best tray for my cable?
As described by the NF 15-100 standard, the antenna cable cannot follow the same path as the low voltage cables. They must be separated by a physical element (e.g. a tube) to ensure insulation, or two different paths can be used.
  • To learn more about NF C 15-100, click here:

Schneider Electric Nigeria