{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to interpret the diagnosis of the LoRa tester?
If there are two bars or less, the signal is too weak to ensure a good level of service. If there are three or four bars, the signal quality is ok.

If you press the screen toggle button on the right side:
•    If UL1 is >= -13db: the LoRa network is good
•    If -13db > UL1 > -20db: the LoRa network is weak and a good level of service is not guaranteed. In this case, we recommend using the cable extender to improve the signal quality level
•    If UL1 < -20db or there is no result (--): the LoRa network is not available

Schneider Electric Nigeria