{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do I know if the wireless panel server is actually connected to the LoRa network?

Article available in these languages: Dutch

You will know if the wireless panel server is connected to the LoRa network if it is already associated with EcoStruxure Facility Expert.
There are two different cases:
If the wireless panel server is already associated with Facility Expert:
  • The LED is solid green: the wireless panel server is connected.
  • The LED is flashing orange: the wireless panel server has lost the LoRa network.
The only way to ensure that the wireless panel server is connected without the association with Facility Expert is to use a LoRa tester. Note that you have the option to perform an eligibility test to estimate your coverage level.

Schneider Electric Nigeria