{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is there an IEC drum sequencer in EcoStruxure Control Expert for the M580 PLC platform ?


Issue:
IEC drum sequencer in EcoStruxure Control Expert for the M580 PLC platform


Product Line:
M580, EcoStruxure Control Expert


Resolution:
No, not in the standard library of Control Expert. Attached is a Drum sequencer DFB that you can use with the M580 PLC platform.

Schneider Electric Nigeria

Attachment(s)
Drum_Sequencer.xdb [4.81 KB]