{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
"Configured" status is not displayed in TGML for Cubicle 5 to Cubicle 16 for SMD (Switchgear Monitoring Device)
Issue
"Configured" status is not displayed (checked or unchecked)  in TGML for Cubicle 5 to Cubicle 16 for SMD (Switchgear Monitoring Device)
image.png
Product Line
PO2021 PSO2020 R2 CU1
Environment
PO2021 / PSO2020R2CU1 with webHMI application having SMD devices
Solution
  1. Close any open webHMI application in browser
  2. Stop IIS from IIS Manager
  3. Navigate to C:\ProgramData\Schneider Electric\Power SCADA Operation\v2021\User\PLS_Include\TGML\Templates\Thermal
  4. Take backup of "Thermal" Folder in v2021 folder and its sub-folders (C:\ProgramData\Schneider Electric\Power SCADA Operation\v2021)
  5. Replace the attached (Related) TGML files in Thermal folder normally located at C:\ProgramData\Schneider Electric\Power SCADA Operation\v2021\User\PLS_Include\TGML\Templates\Thermal
  6. If your installation location is different, please make sure you replace these files in Power SCADA Operation\v2021\User\PLS_Include\TGML\Templates\Thermal
  7. Start IIS Manager
  8. Open the TGML for SMD and verify the "Configured" Status visible for all Cubicles.
  9. If not able to view updated TGMLs , perform iisreset using Command Prompt (Required Administrator privileges).

Schneider Electric Nigeria

Attachment(s)
Thermal tgml files.zip [759.01 KB]
Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: