{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is there a way to get an ATV320 ATV Logic print out in SoMove?

Issue:
Can you print your ATV Logic configuration from SoMove Software?


Product Line:
Altivar 320


Environment:
All Models


Cause:
ATV Logic


Resolution:
There is no print function available for ATV Logic like there is for parameters. Will have to do screen capture is the only way to print ATV Logic

Schneider Electric Nigeria